CW PA10.4 can not use flash programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW PA10.4 can not use flash programmer

ソリューションへジャンプ
71,369件の閲覧回数
markxu
Contributor I

     i can use the flash programmer in CW PA10.0 and CW PA10.1,bu can not use in CW PA10.3 and CW PA10.4,the button “ADD” is blank.

ラベル(1)
0 件の賞賛
返信
1 解決策
71,241件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello  xu xiaolong,

This is a compatible problem for eclipse plugin on Chinese edition OS, please check whether change "appearance" of your system could be helpful.

If it doesn't help, you have to install English edition OS, if you want to use CodeWarrior 10.4.

Actually you could continue to use CodeWarrior 10.1.1, what specific features do you need? For new target boards?

Thanks,

Yiping

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
71,242件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello  xu xiaolong,

This is a compatible problem for eclipse plugin on Chinese edition OS, please check whether change "appearance" of your system could be helpful.

If it doesn't help, you have to install English edition OS, if you want to use CodeWarrior 10.4.

Actually you could continue to use CodeWarrior 10.1.1, what specific features do you need? For new target boards?

Thanks,

Yiping

0 件の賞賛
返信
71,241件の閲覧回数
markxu
Contributor I

thanks so much,you're right,when i change the OS regional,CW 10.4 works properly.

0 件の賞賛
返信