CW PA10.4 can not use flash programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW PA10.4 can not use flash programmer

Jump to solution
71,432 Views
markxu
Contributor I

     i can use the flash programmer in CW PA10.0 and CW PA10.1,bu can not use in CW PA10.3 and CW PA10.4,the button “ADD” is blank.

Labels (1)
0 Kudos
Reply
1 Solution
71,304 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello  xu xiaolong,

This is a compatible problem for eclipse plugin on Chinese edition OS, please check whether change "appearance" of your system could be helpful.

If it doesn't help, you have to install English edition OS, if you want to use CodeWarrior 10.4.

Actually you could continue to use CodeWarrior 10.1.1, what specific features do you need? For new target boards?

Thanks,

Yiping

View solution in original post

0 Kudos
Reply
2 Replies
71,305 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello  xu xiaolong,

This is a compatible problem for eclipse plugin on Chinese edition OS, please check whether change "appearance" of your system could be helpful.

If it doesn't help, you have to install English edition OS, if you want to use CodeWarrior 10.4.

Actually you could continue to use CodeWarrior 10.1.1, what specific features do you need? For new target boards?

Thanks,

Yiping

0 Kudos
Reply
71,304 Views
markxu
Contributor I

thanks so much,you're right,when i change the OS regional,CW 10.4 works properly.

0 Kudos
Reply