CW 5.2 for HCS12(x)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 5.2 for HCS12(x)

2,427件の閲覧回数
tnriley
Contributor III

I have been able to get a node locked licensed version of CW 5.1 to run correctly on a non-networked win7-64 machine. I have attempted to download the version 5.2 update and install on the same machine. However, the 5.2 version does not have all of the processor options available that are included in 5.1 version. In fact it is a greatly limited listing of those available in 5.1. Is there another download somewhere that I am missing?

 

I am using this page for downloads

CodeWarrior for HC12 Professional Edition WIN

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=7153847 

 

Also, is there a method to perform an update rather than a new install from 5.1 to 5.2? This is a non-networked machine.

ラベル(1)
0 件の賞賛
返信
1 返信

2,315件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tim,

CW 5.2 can only support limited device.  this is a market decision.

 

This release includes support for the following derivatives:
    - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96
    - MC9S12G128, MC9S12G96
    - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64
    - MC9S12GN16, MC9S12GN32
    - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128
    - MC9S12XEP100, MC9S12XEP768
    - MC9S12XEQ384, MC9S12XEQ512
    - MC9S12XET256
    - MC9S12XS128, MC9S12XS256, MC9S12XS64
    - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64

 

I wrote an article about how to install missing device to CW v5.2

https://community.freescale.com/docs/DOC-330657


My suggestion for you is to use CW5.1 instead. attached is how to download CW5.1. Hope this helps.

 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------