CW 10.5 problems with downloading and debugging - Coldfire

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.5 problems with downloading and debugging - Coldfire

1,438件の閲覧回数
admin
Specialist II

Hi.

 

I just recently upgraded my machine on work for a newer model with a bit more horepower under the hood and win7 64bit instead of XP.

 

I have now run into quite a problem. I dont seem to be able to debug on the code for the coldfire MCU's i'm using. download has also become increasingly problematic, i cant seem to locate the issues.

on the old machine i used 10.2 installed by med predecessor in the company, so i havent got any experience with setting up the IDE is this is needed.

 

Hope somebody can help me out.

 

It show a error message telle me that GDI cant connect to hardware memory.

 

i cant show you this error since i ran into a compiler error while trying to work out the kinks...

8381_8381.pngUdklip.PNG.png

 

Michael.

ラベル(1)
0 件の賞賛
返信
1 返信

1,327件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

try these two:

1. go to CW menu"project", "clean" to remove the old association then rebuild the project.

2. if the project still exists, remove .metadata folder in currently workspace then reopen CW. "clean " and rebuild the project again.

0 件の賞賛
返信