CW 10.4 connectivity issue with T4240RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.4 connectivity issue with T4240RDB

2,127件の閲覧回数
b48252
NXP Employee
NXP Employee

I am trying to flash u-boot on T4240RDB box using CW . I installed CW 10.4 and connected with USB TAP with JTAG port

 

Also as per document I have changed the jumper setting.

 

I have created new project in the CW 10.4 IDE and while trying to connect to the T4240RDB facing below issue.

 

15727_15727.jpgcw_issue.jpg

 

 

Please share the exact procedure to use CW10.4 with T4240RDB using USB TAP.

 

Best Regards,

Manish Tiwari

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,011件の閲覧回数
catalindemergia
Contributor IV

Hello,

first of all, have you configured the connection to USB ?

Debug Configurations/Edit Connection and choose "USB TAP" from the Connection Type combo.

Don't use CW tap or anything else, because your hardware is USB Tap.

regards,

Catalin

0 件の賞賛
返信

2,011件の閲覧回数
b48252
NXP Employee
NXP Employee

Yes, I am using USB TAP option.

Please share the full procedure or any document so it will be helpful.

Best Regards,

Manish Tiwari

0 件の賞賛
返信

2,011件の閲覧回数
catalindemergia
Contributor IV

Hello,

You can check the Targeting_PA_Processors.pdf document in your CW installation folder

(PA\Help\PDF)

regards,

Catalin

0 件の賞賛
返信