CW 10.3 & DEMO9S08SF4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.3 & DEMO9S08SF4

2,308件の閲覧回数
ecb
Contributor II

Hi;

 

I have troubles with CW10.3 & DEMO9S08SF4 (OSBDM) under Win 7 64 bits.

 

The driver seems to be well instaled:

 

9897_9897.jpgsf4_3.jpg

But there is no connection:

9898_9898.jpgsf4_1.jpg

9899_9899.jpgsf4_2.jpg

Some help please?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,057件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

I would suggest using the latest CW v10.5 for your development!

regarding to your problem, it seems to be a driver issue.

could you please uninstall item "LiUSB-Win32 Devices-> OSBDM/OSJTAG-..." and "Ports(COM & LPT) ->OSBDM/OSJTAG-CDC Serial port..." in Device Manager of your Windows system.

and then re-plug your board to let the PC find the driver automatically (usually, it will find several versions driver, please select the latest version).

hope it helps!

0 件の賞賛
返信

2,057件の閲覧回数
ecb
Contributor II

Hello,

CW 10.5 installed, driver automatically installed:

OSBDM_drv_1.jpg

But the issue is the same :smileysilly:

0 件の賞賛
返信

2,057件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hello ecb,

I'm sorry  for my delay response!

if the problem is still remains, then, I would suggest update the firmware of OSBDM of your demoboard.

the updater is available at:

P&E Microcomputer Systems

Please click "Firmware Updates & Recovery" to download the updater.

then connect demoboard to PC and run the updater, follow the instructions to update.

I hope it helps!

0 件の賞賛
返信