CPU is B4860. Error: CCSProtocolPlugin: Fail to correctly configure the JTAG chain. 

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU is B4860. Error: CCSProtocolPlugin: Fail to correctly configure the JTAG chain. 

1,205件の閲覧回数
荥芸吴
Contributor I

The RCW saved in Flash is corrupted. Then the CW has the error and can't connect to the board. I didn't find the JTAG Chain file with RCW in CodeWarrior. Could you please provide a JTAG Chain file with RCW? Or help me to solve the issue?

 

Thanks so much!

ラベル(1)
0 件の賞賛
返信
1 返信

1,081件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

CodeWarrior JTAG configuration file overriding RCW is not available for B4860.

Please use hard-coded RCW to setup your target board.

cfg_rcw_src[0:8]=0b0_1000_0110

The device can be initialized with a hard-coded RCW option, selected by the cfg_rcw_src[0:8] configuration inputs (which are multiplexed on the {IFC_AD[8:15], IFC_CLE} pins).

If you use B4860QDS demo board, please configure SW3[0-7]=01000011.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信