CODE WARRIOR IDE SOFTWARE.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CODE WARRIOR IDE SOFTWARE.

2,625 Views
jatinmehta
Contributor I

Hi,

I am using the above mentioned software. This software is not reading header files like  #include "SD.h" , #include "FAT.h" .

Also i am using uC MPC5606B ,and when i include the header file #inlcude "MPC5606B.h",it doesnot identify ADC.

Can someone suggest some tips.

Thanks in advance.

Labels (1)
0 Kudos
Reply
3 Replies

2,489 Views
TICS_Fiona
NXP Employee
NXP Employee

Could you please check the compiler settings for head file search path?

If this does not help, could you please attach a simple project to help us reproduce the error? Thanks!

0 Kudos
Reply

2,489 Views
jatinmehta
Contributor I

hi,TICS_Fiona

I have attached the project do see and any suggestions are welcome.

thanks.

0 Kudos
Reply

2,489 Views
trytohelp
NXP Employee
NXP Employee

Hi Jatin,

Unfortunately nothing was attached to your post.

Can you check it again ?

If you've problem you can post your problem to the Customer Service Request process.

  - Go to following URL: http://www.freescale.com/TechSupport

  - Click on Submit a Service Request. You will come to a login page.

  - If you are already registered with Freescale (using the Forum, subscribed to newsletter, ...) use your Freescale login and password. Otherwise, Click on "Register Now" to get registered.

  - You can submit your request through the web from there.

Regards

Pascal

0 Kudos
Reply