CMSIS library and Kinetis in CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS library and Kinetis in CodeWarrior

4,617件の閲覧回数
ViniciusHoff
Contributor II

I want use the CMSIS-DSP library to calculate the real FFT of a signal, but when I call the FFT functions and I compile in CodeWarrior, the code size exceeds the flash memory.

I´m using a MK20DX128VLH5 with 128kB of flash and my code without FFT function has 6kB.

 

FFT functions of the library are so great right? Is it correct this?

Don´t have a reduce form of FFT functions to use with Kinetis?

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,800件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hi Vinicius

Any update regarding implementation of the library?

Regards

Amit Kumar

0 件の賞賛
返信

3,800件の閲覧回数
ViniciusHoff
Contributor II

Hi Amit Kumar

No, I gave up on implement the library. The code with CMSIS-DSP FFT is very big and I am not able to reduce it.

Regards

Vinícius Hoff

0 件の賞賛
返信

3,800件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hi Vinicius

I figured a way how to implement CMSIS lib in Codewarrior please refer to the following post Interfacing CMSIS Library in Codewarrior? You don't need to impement the entire library as it is really huge. but you can implement the CMSIS functions and related lib in your project. Hope It helps

Best Regards

Amit Kumar

3,800件の閲覧回数
ViniciusHoff
Contributor II

Thank you Amit Kumar,

I'll try to implement the library again.

0 件の賞賛
返信

3,800件の閲覧回数
ViniciusHoff
Contributor II

I´m using the library file "libarm_cortexM4l_math.a", available in the folder /Lib/GCC. There are a "arm_cortexM4l_math.lib" in the folder /Lib/ARM.

What´s the difference between them?

0 件の賞賛
返信

3,800件の閲覧回数
fitch
Contributor I

The "libarm_cortexM4lf_math.a" library is for mcu's with a hardware FPU. The "libarm_cortexM4l_math.a" library is for ones without hardware FPU.

0 件の賞賛
返信