CMSIS and Codewarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMSIS and Codewarrior

3,876件の閲覧回数
tobiashofbaur
Contributor I

Hello,

for an ARM Cortex M4 project, i want to use the CPU specific instructions for sqrt using the ARM Toolchain  with the ARM Compiler.

I can sucessfully include CMSIS into the project, however, it seems, that the necessary macros are not generated (e.g. compiler etc.)

Moreover, if I strip everything unnecessary from CMSIS and onyl include the bare VSQRT in the syntax of CMSIS

      __asm("VSQRT.F32 %0,%1" :  "=t"(*pOut) : "t"(in));   (wrapped in a function)

the compiler complains about the constraints.

Do you know what is going wrong, or what I have to change? Unfortunately i cannot find a detailed documentation on the Freescale Arm Compiler or the vsqrt.

Thanks

Tobias

タグ(2)
0 件の賞賛
返信
6 返答(返信)

3,562件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tobias,

Which Cortex M4 MCU are you using?


Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

3,562件の閲覧回数
tobiashofbaur
Contributor I

Hi Carlos,

thank you for the reply.

It is a MK70FX512VMJ15

0 件の賞賛
返信

3,562件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tobias,

I think that the following post created by our colleague Erich Styger might be helpful for you, it explains the usage of the ARM CMSIS Libraries with Kinetis in CodeWarrior:

Tutorial: Using the ARM CMSIS Library | MCU on Eclipse 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

3,562件の閲覧回数
tobiashofbaur
Contributor I

Hi Carlos,

I followed that example, and it works as far as it is applicable. However in our project we cannot use the GCC compiler, but have to use the Freescale ARM Compiler ( mwccarm )

It seem, this does not generate the necessary macros for cmsis to work/ does not recognize the cmsis syntax.

Best

Tobias

0 件の賞賛
返信

3,562件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Tobias,

 

Which errors are you getting? Could you share an example project so I can replicate this on my side?


Thanks in advance for your response!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

3,562件の閲覧回数
tobiashofbaur
Contributor I

Hi Carlos,

I attached a minimal "working" example. The project has the same setting as our main project.

As it is, it does not compile. If I comment the asembler line, it does compile.

If I change the compiler to ARM Ltd Windows GCC Compiler, it does compile with the asembler line.

Thank you for your help

Best

Tobias

0 件の賞賛
返信