CCSAPI Protocol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCSAPI Protocol

2,465 Views
michaelmeier
Contributor II

Is there any information available on the CCSAPI TCP protocol spoken between CCS and CodeWarrior?

 

The reason I am asking is that I would like to read out data from my MCU's address space in real time. With BDM being an advanced debugging solution, I believe it's technically possible to read from a processor's address space while the processor keeps executing software practically uninterrupted. I would like to use the CCSAPI to programmatically gain access to the RAM of my processor and read out profiling logs (generated by my own profiler) in real time.

Labels (1)
0 Kudos
Reply
4 Replies

2,284 Views
trytohelp
NXP Employee
NXP Employee

Hi Michael,

I got feedback from dev team.

Unfortunately we don't have documentations for CCS API/protocol used to establish communication between hardware(board/interface) and debugger.

To have information I recommend you to launch or open the CCS and execute the command: log verbose

Regards

Pascal

0 Kudos
Reply

2,284 Views
michaelmeier
Contributor II

Hi Pascal

Thank you. The hint regarding the log command is most helpful.

Cheers

Michael

0 Kudos
Reply

2,284 Views
trytohelp
NXP Employee
NXP Employee

Hi Michael,

You're welcome.

Unfortunately we can not provide more info.

Pascal

0 Kudos
Reply

2,284 Views
trytohelp
NXP Employee
NXP Employee

Hi Michael,

Sorry for the delay.

I think we don't provide this type of information.

I've contacted the development team and will keep you informed.

Regards

Pascal

0 Kudos
Reply