CAN reciever interrupt flage problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN reciever interrupt flage problem

1,864 Views
kdn
Contributor III

I am using CAN module of MC9S12XHZ512 microcontroller, I successfully archive transmitting of data from my microcontroller, but problem is that I am able to receive data only one time after that my controller get hang, I think that I have not clear my CAN receiver  interrupt flag, can anyone tell me where I can get CAN receiver interrupt flag in datasheet, I post my interrupt code for CAN below. Do MC9S12XHZ512 compiler support sprintf function.

 

 

#pragma CODE_SEG __NEAR_SEG NON_BANKED

 

 

interrupt void Vcan1RxISR(void)

 

{

     unsigned char  RxBuffer[8],u8Length=8;

   

    unsigned int R,temp;

   

    LCD_Cmd(0x80);

 

     R = CAN1RXDSR0;

    

       

    

         Convert(R);

         LCD_Data(D);

         delay();

         LCD_Data(C);

         delay();

         LCD_Data(B);

         delay();;

         LCD_Data(A);

         delay();

                       

      PORTA = 0xFF;

    

        

      CAN1RFLG_RXF = 1;

}

Labels (1)
0 Kudos
Reply
2 Replies

1,725 Views
TICS_Fiona
NXP Employee
NXP Employee

The Receive Buffer Full Flag(RXF) is bit 0 in MSCAN Receiver Flag Register (CANRFLG).

After the CPU has read that message from the RxFG buffer in the receiver FIFO, the RXF flag must be cleared to release the buffer.

For details, please see section 14.3.2.5 in data sheet:

http://cache.freescale.com/files/microcontrollers/doc/data_sheet/MC9S12XHZ512.pdf

And MC9S12XHZ512 compiler supports sprintf function, please include the head file <stdio.h>.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,725 Views
kdn
Contributor III

RXF indicate Receiver FIFO get full , I am looking for CAN Receiver interrupt flag.

Thanks for sprintf function

0 Kudos
Reply