CAN communication on my demo boards DEMO9S12XDT512 using code warrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN communication on my demo boards DEMO9S12XDT512 using code warrior

3,444件の閲覧回数
ilyasselmoutia
Contributor II

Hello 

If possible,I want to test CAN communication on my demo boards DEMO9S12XDT512 using code warrior tool , i don't new how and idon't even have de source code ,,.

0 件の賞賛
返信
5 返答(返信)

3,109件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ilyass elmoutia ,

Please have look at MCSCAN driver for S12(X) devices :

S12XD MCUs|16-Bit Microcontroller|NXP 

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,109件の閲覧回数
ilyasselmoutia
Contributor II

think you it's very helpful and i hope you may helpe me more this time with

configuring my card to analyze a CAN BUS ,i'm a beggener thinks again

<https://www.avast.com/sig-email?utm_medium=email&utm_source=link&utm_campaign=sig-email&utm_content=webmail>

Garanti

sans virus. www.avast.com

<https://www.avast.com/sig-email?utm_medium=email&utm_source=link&utm_campaign=sig-email&utm_content=webmail>

<#DAB4FAD8-2DD7-40BB-A1B8-4E2AA1F9FDF2>

2018-02-28 10:18 GMT+01:00 Alice_Yang <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: CAN communication on my demo boards DEMO9S12XDT512 using code warrior

reply from Alice_Yang

<https://community.nxp.com/people/Alice_Yang?et=watches.email.thread> in *CodeWarrior

Development Tools* - View the full discussion

<https://community.nxp.com/message/990930?commentID=990930&et=watches.email.thread#comment-990930>

0 件の賞賛
返信

3,109件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

Sorry , could you please describe your problem in detaly.

For beggener, I recommend you first run demo code on your side.

Hope it helps

Alice

0 件の賞賛
返信

3,109件の閲覧回数
ilyasselmoutia
Contributor II

Hello Alice thank you for your hellp ,it's very nice gesture from you ,

i hope if you may send me the PROJECT of the CAN BUS communication for

DEMO9SX12DT512.

i just need to send and receive a message to and from the CAN BUS ,

it's ganna be a big helpe for my school project.

this is my Email: [email protected]

thank you a again

ilyass elmoutia

<https://www.avast.com/sig-email?utm_medium=email&utm_source=link&utm_campaign=sig-email&utm_content=webmail>

Garanti

sans virus. www.avast.com

<https://www.avast.com/sig-email?utm_medium=email&utm_source=link&utm_campaign=sig-email&utm_content=webmail>

<#DAB4FAD8-2DD7-40BB-A1B8-4E2AA1F9FDF2>

2018-03-01 8:00 GMT+01:00 Alice_Yang <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: CAN communication on my demo boards DEMO9S12XDT512 using code warrior

reply from Alice_Yang

<https://community.nxp.com/people/Alice_Yang?et=watches.email.thread> in *CodeWarrior

Development Tools* - View the full discussion

<https://community.nxp.com/message/991329?commentID=991329&et=watches.email.thread#comment-991329>

0 件の賞賛
返信

3,109件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ilyass,

Sorry there isn't a demo  exactlly for this chip, while the  chips in S12 family basically the same.

you can refer to demo of "msCAN Driver XEP100" .

BR

Alice

0 件の賞賛
返信