CADE WARRIOR FOR MAC OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CADE WARRIOR FOR MAC OS

2,624 Views
jashandeepsingh
Contributor I

HELLO GUYS,
I M USING MAC AND I NEED CODE WARRIOR BUT I CANT FIND ANYTHING FOR MAC ON WEBSITE.
PLEASE HELP ME OUT

0 Kudos
Reply
5 Replies

2,539 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

2,539 Views
jashandeepsingh
Contributor I

MC9S12E128 thanks

On Mon, Jul 10, 2017 at 12:26 PM Carlos_Mendoza <[email protected]>

0 Kudos
Reply

2,539 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jashandeep.

For the moment, the latest CW version that can support MC9S12E128 is CW for hcs12(x) v5.1. It doesn't support MAC OS. unfortunately, there is not a CW version can support MC9S12E128 on MAC OS.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,539 Views
jashandeepsingh
Contributor I

Thank you so much for your time sir .

I will look for another windows machine now.

Have good day.

On Wed, Jul 12, 2017 at 12:38 AM ZhangJennie <[email protected]>

0 Kudos
Reply

2,539 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Have a great day,
Jennie Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply