Build error: identifier expected...?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build error: identifier expected...?

1,680件の閲覧回数
bjornverbrugge
Contributor I

Hi,

 

 

I'm tying to initialize a uart of an MK22FX512 using PE and CW10.6 but the generated code runs into two a build errors.

 

29772_29772.JPGCapture.JPG29773_29773.JPGCapture1.JPG29774_29774.JPGCapture2.JPG

Does this sound familiar to anybody...?

 

Thank a lot!

Bjorn

ラベル(1)
0 件の賞賛
返信
1 返信

1,560件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Could you please attach a simple example project to reproduce the problem? Or attach a screenshot for the PE component properties.

In addition, the latest CW version is v10.6.4, it is now available on the Freescale WEB at www.freescale.com/cwmcu10.

This is a full release and includes all the previous updates (Update 1, Update 2 and Update 3) in a single installation.

Further information and the release notes are available on the following Freescale community page:

https://community.freescale.com/docs/DOC-104810

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信