Bean vs Component

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bean vs Component

1,639 次查看
davidzhou
Contributor V

Hi,

I have MC9S12C64CFA25, with Code Warrior Classic v5.9.0 installed. 

I am a newbie on Code Warrior classic. The PE generated code is commented as:

**     THIS COMPONENT MODULE IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
**     Filename  : AD1.c
**     Project   : TestA
**     Processor : MC9S12C64CFA25
**     Component : ADC
**     Version   : Component 01.630, Driver 01.19, CPU db: 2.87.403
**     Compiler  : CodeWarrior HC12 C Compiler
**     Date/Time : 5/4/2017, 1:46 PM

But the original project generated with comments (from a different PC):

**     THIS BEAN MODULE IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
**     Filename  : Vectors.C
**     Project   : FS200_V
**     Processor : MC9S12C64CFA25
**     Version   : Bean 02.001, Driver 02.01, CPU db: 2.87.395
**     Compiler  : CodeWarrior HC12 C Compiler
**     Date/Time : 8/13/2010, 11:25 AM
**     Abstract  :
**         This bean "MC9S12C32_48" implements properties, methods,
**         and events of the CPU.

I guess they are similar. But I prefer to generate code as bean-beased, instead of component-based. How to make a selection for bean-based code generation? I have seen bean library in the installation folder. Do I need to enable or something?

Thank you,

David Zhou

0 项奖励
回复
2 回复数

1,509 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi David,

Roughly, we can classify processor expert components as CPU component and non-CPU component.

for non-CPU component (for example ADC component), we can right click then choose "don't write generated component modules". thus all this component generated files will not be overwritten.

pastedImage_1.png

However this feature can't work for CPU component.

Does this answer your question?

 
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,509 次查看
davidzhou
Contributor V

Hi Jennie,

Thank you for your reply.

Sorry I didn't state my question clearly. My project is created by someone else long timer ago with classic V5.0.

Now I am using classic V5.2. With V5.0 all PE component code is generated as beans, while V5.2 is generated as components. They are not in the same format. For example, #define TIMER_INTERVAL 0x10U for bean code

while component code may be in the format of #define TIMER_INTERVAL 16.

Because we have made many changes to the generated code, it is very difficult to find the differences if generated code is in different format. So I want to have the same format as the previous V5.0. Your web site only has V5.2 classic available to download.

Thank you,

David Zhou

0 项奖励
回复