Authentication error in NXP Library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Authentication error in NXP Library

5,513件の閲覧回数
raj_shinde
Contributor I

I am developing an android app to authenticate mifare UltraLightC chip ,but the problem i am facing while authenticating  chip is , it always  throws an exception, every time even if it is authenticated or not (i.e .authenticate() method  of NXPlibrary), and how can we confirm that our key is being successfully authenticated as per an example in  datasheet provided by mifare, they are just using an log below the .authenticate() method so, is this a proper way to authenticate an key ?  while debugging i found that this method always throws an exception message(i.e NxpNFCLibException)  rather than ideally an authenticating method should give an response for example authenticated true or false, it do not return anything, so how can we confirm whether our key is properly authenticated  i am attaching my debugging logs with it ? Please provide me a solution or an example  on how to authenticate key and how to check whether it is authenticating properly or not ? 

Version of NXP Library  i am using 

nxpnfcandroidlib-1.7

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

5,309件の閲覧回数
marcoperrone
Contributor I

Hi  to all,

I tried to use the code suggested by NXP TechSupport @jimmychan to authenticate a Mifare Ultralight C with an Android smartphone.
Here the the data between the the app and the tag:

My Key is: 42 52 45 41 4B 4D 45 49 46 59 4F 55 43 41 4E 21

I start communication  TAG : 1A 00

The TAG answer with (encoded) RndB: AF 69 EC C8 F7 CA DC 1A C8

so the the IV for next communication become: 69 EC C8 F7 CA DC 1A C8

the RndB (decoded) is: CB 0C AC EE F2 76 F1 7E

the RndB' (rotate) is: 0C AC EE F2 76 F1 7E CB

the RndA is: C9 60 0A DC EB 08 FD C4

The value sent to the tag is: AF encoded (RndA + RndB')

AF 90 79 9A 6D 73 E9 51 49 C7 AA 66 D9 0C 08 BE C5

When I sent this I have an exception Transceive failed (like the data sent is not correct)

I check on this site http://tripledes.online-domain-tools.com/

And the value sent is correct

I hope You can help me

Best Regards

Marco

0 件の賞賛
返信

5,418件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

5,304件の閲覧回数
marcoperrone
Contributor I

Hi @jimmychan,

Did You use the code suggested successfully, because I have an exception during the authentication, I explained all in my other post.
Thank You 

Best Regards

Marco

0 件の賞賛
返信