Assembly Language debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Assembly Language debugger

1,723件の閲覧回数
scarr
Contributor I

Hi, Can Codewarrior be used as a assembly language debugger? what I mean by this is connect to a device via BDM single step through code without having a project or debug files / support files, just a ROM image.

 

Thanks

 

Steve

ラベル(1)
0 件の賞賛
返信
1 返信

1,622件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Steve:

Sure this is possible with CodeWarrior. You still need a dummy project to hold your debug configuration, but just select "Connect" as session type in CodeWarrior. Check the next tutorial by our colleague Erich Styger:

Hot-Sync: Attach, Connect & Download | MCU on Eclipse

Just be aware that the tutorial was for an earlier version of CodeWarrior (I think it was CW v10.3). In CW v10.5, or the latest version 10.6 lauched a couple of days ago, you will have something like this:

Debug_session.png

Hope this helps


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信