Assembly Language debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assembly Language debugger

1,693 Views
scarr
Contributor I

Hi, Can Codewarrior be used as a assembly language debugger? what I mean by this is connect to a device via BDM single step through code without having a project or debug files / support files, just a ROM image.

 

Thanks

 

Steve

Labels (1)
0 Kudos
Reply
1 Reply

1,592 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Steve:

Sure this is possible with CodeWarrior. You still need a dummy project to hold your debug configuration, but just select "Connect" as session type in CodeWarrior. Check the next tutorial by our colleague Erich Styger:

Hot-Sync: Attach, Connect & Download | MCU on Eclipse

Just be aware that the tutorial was for an earlier version of CodeWarrior (I think it was CW v10.3). In CW v10.5, or the latest version 10.6 lauched a couple of days ago, you will have something like this:

Debug_session.png

Hope this helps


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply