Apply a license.datbecause of exceeding the amount of code during download.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Apply a license.datbecause of exceeding the amount of code during download.

769件の閲覧回数
珠莉袁
Contributor I

Hello,

    I would like to apply for an evaluation version of the license. Because I have applied  the evaluation version CD5.1 , The process always remind exceed the amount of code during the download.

ラベル(1)
0 件の賞賛
返信
1 返信

626件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

The Evaluation Edition of CodeWarrior can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X

After installation, the license is included in CodeWarrior folder.

Or please send mail to support@freescale.com to apply an evaluation license.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信