Apply a license.datbecause of exceeding the amount of code during download.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Apply a license.datbecause of exceeding the amount of code during download.

787 Views
珠莉袁
Contributor I

Hello,

    I would like to apply for an evaluation version of the license. Because I have applied  the evaluation version CD5.1 , The process always remind exceed the amount of code during the download.

Labels (1)
0 Kudos
Reply
1 Reply

644 Views
TICS_Fiona
NXP Employee
NXP Employee

The Evaluation Edition of CodeWarrior can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X

After installation, the license is included in CodeWarrior folder.

Or please send mail to support@freescale.com to apply an evaluation license.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply