AppTRK.elf generation for P4080DS (Code warrior version 10.5)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AppTRK.elf generation for P4080DS (Code warrior version 10.5)

ソリューションへジャンプ
5,530件の閲覧回数
rahul011189
Contributor I

I am working with P4080DS and Code warrior 10.5. I am trying to debug a linux application.

As per the code warrior documentation, I need to run AppTRK.elf on the target Linux system but it doesn't describe on how to generate the AppTRK.elf file.

Please assist me on generating the same.

 

Thanks,

Rahul

ラベル(1)
0 件の賞賛
返信
1 解決策
5,355件の閲覧回数
addiyi
NXP Employee
NXP Employee

Building apptrk for p4080ds works fine for me. Attached you can find exported_flags script that I used. Please modify the path and source this script before build the apptrk.

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
5,355件の閲覧回数
addiyi
NXP Employee
NXP Employee

There are two ways to generated the apptrk,elf.

1. Build the apptrk sources provided in CodeWarrior (Freescale\CW_PA_v10.5.0\PA\PA_Tools\AppTRK\)

2. If you use SDK to build your linux images, add apptrk in build recipe.

Adrian

0 件の賞賛
返信
5,355件の閲覧回数
rahul011189
Contributor I

Hi Adrian,

Thanks for the prompt reply.

I tried method 1 before posting the question itself. But I am getting errors when I am trying to use MAKE for the source present at:

Freescale\CW_PA_v10.5.0\PA\PA_Tools\AppTRK

Is there something that I am missing? Any specific step that needs to be performed for build AppTRK source code?

Regards,

Rahul

0 件の賞賛
返信
5,355件の閲覧回数
addiyi
NXP Employee
NXP Employee

Did you use correct cross toolchain when building apptrk? Could you share the errors you get when building?

Adrian

0 件の賞賛
返信
5,355件の閲覧回数
rahul011189
Contributor I

I don't think the error is related to toolchain. Please see the following error log.

I followed the steps in Freescale\CW_PA_v10.5.0\PA\PA_Tools\AppTRK\appTRK\INSTALL.

The configuration step is successful but MAKE is throwing errors.

App_TRK.png

0 件の賞賛
返信
5,355件の閲覧回数
rahul011189
Contributor I

Hi Adrian,

Can you please assist me with the issue?

Regards,

Rahul

0 件の賞賛
返信
5,355件の閲覧回数
addiyi
NXP Employee
NXP Employee

Hi Rahul,

Did you use ./configure? Could you share configure command? Did you build libelf before building apptrk?

Adrian

0 件の賞賛
返信
5,355件の閲覧回数
rahul011189
Contributor I

As I mentioned the configuration step was correct. The ./configure did not throw any errors. And yes libelf was built.

0 件の賞賛
返信
5,355件の閲覧回数
rahul011189
Contributor I

Adrian,

Please see the snapshot for ./configure step.

configure.png

0 件の賞賛
返信
5,356件の閲覧回数
addiyi
NXP Employee
NXP Employee

Building apptrk for p4080ds works fine for me. Attached you can find exported_flags script that I used. Please modify the path and source this script before build the apptrk.

Adrian

0 件の賞賛
返信
5,355件の閲覧回数
rahul011189
Contributor I

Hi Adrian,

I tried the same steps as you mentioned over and over again but I kept getting errors in the source files.

But after removing the apptrk folder and regenerating it from the back up .tar file, I was able to generate the AppTRK.elf file with the same sequence I was trying earlier. Not sure what the problem really was.

Anyways, the problem is solved. Thank you very very much for your support.

Regards,

Rahul

0 件の賞賛
返信