Any major differences between CW USB TAP and CW TAP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Any major differences between CW USB TAP and CW TAP?

2,175 次查看
mariochan
Contributor I

Hi Tech support,

 

I previously purchased CW USB TAP.

 

Probe Tip:  Power Architecture JTAG/COP

PC window 7 64 bit.

PC installed Power Architecture 8.8

 

Target PCB with the processor: MPC8358ECVRAGDGA

 

It worked. Typed "findcc utaps" @ CCS, it shows my CW USB TAP serial number.

I am able to "erase" in flash programmer.

 

Problem:

I purchased CW TAP (Supports USB and Ethernet)  for mass production.

PC window 7 64 bit. (Same)

PC installed Power Architecture 8.8 (Same)

 

Target PCB with the processor: MPC8358ECVRAGDGA (Same)

 

It failed. Typed "findcc utaps" or "findcc ethaps", etc @ CCS. It does not show anything.

I am NOT able to "erase" in flash programmer, it shows check JTAG clock speed.

 

 

i have set netparam as following:

 

core> netparam

ethernet_address        = 00:04:9F:03:9B:ED

bootconfig              = static:FSL039BED

static_ip_address       = 169.254.3.4

static_dns_server       = <none>

static_hosts            = <none>

static_routes           = <none>

 

 

PC directly connects to CW TAP.

PC's ip= 169.254.3.2

PC's subnet mask= 255.255.0.0

 

 

Please advise.

标签 (1)
0 项奖励
回复
3 回复数

1,962 次查看
addiyi
NXP Employee
NXP Employee

The correct command for finding cwtap in ccs is: findcc cwtaps. Because you are using an old version of CW, it is possible that your ccs version to not support cwtap. Here is a document showing how to update ccs for cwtap usage (it is  not for your version of CW, but is applicable).

Adrian

0 项奖励
回复

1,962 次查看
mariochan
Contributor I

Hi Adrian,

Which version should i use for supporting cwtap?

Current version is Power Architecture 8.8.

My company also has version Power Architecture 10.0.2. Does it support cwtap?

If not, which version should i get?

Thanks for the support.

Mario

0 项奖励
回复

1,962 次查看
addiyi
NXP Employee
NXP Employee

Hi Mario,

The latest version of CodeWarrior is 10.5, and this is the version recommended. But, you can follow the steps from the doc, and use a version of ccs that supports cwtap in your CW 8.8 version.

Also, you can check if your PA 10.0.2 supports cwtap, by opening ccs and probe the command: findcc cwtaps.

Adrian

0 项奖励
回复