Any idea why CW thinks a } is missing at the line with the larger font?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any idea why CW thinks a } is missing at the line with the larger font?

811 Views
danbocko
Contributor I

Any idea why CW thinks a } is missing at the line with the larger font? 

Thanks

Dan

#include <hidef.h>    // common defines and macros */
#include "derivative.h"   // derivative-specific definitions */
#include "stdio.h"
#include "float.h"

#define SPI_isr 0xFFDE
#define ATDCH 0x08    // select ATD ch
#define SW2  PTP_PTP3
#define SW3  PTP_PTP2
#define SW4  PTP_PTP1
#define SW5  PTP_PTP0
#define PBSW PTP |= 0xF0  // PBSW status in PTP low nibble
#define DPSW1 PORTB_PB7
#define DPSW2  PORTB_PB6
#define DPSW3 PORTB_PB5
#define DPSW4 PORTB_PB4
#define DPSW5 PORTB_PB3
#define DPSW6 PORTB_PB2
#define DPSW7 PORTB_PB1
#define DPSW8 PORTB_PB0
#define DPSW PORTB
#define LED1 PORTA_PA0  // LED1 assigned to D9
#define LED2 PORTA_PA1 
#define LED3 PORTA_PA2 
#define LED4 PORTA_PA3 
#define LED5 PORTA_PA4 
#define LED6 PORTA_PA5 
#define LED7 PORTA_PA6 
#define LED8 PORTA_PA7  // LED8 assigned to D2
#define LEDS PORTA

void main(void) {
 
 
 //DisableInterrupts;
 PORTA = 0xFF;     // init porta, all leds off
 DDRA = 0xFF;     // porta output
 PTP = 0xFF;      // init portp 
 DDRP = 0xF0;     // ptp[3:0] input
 PERP = 0x0F;     // enable pulls
 PPSP = 0x00;     // pull-downs
 PIFP = 0xFF;     // clr spurious flags
 PORTB = 0x00;     // init PORTB
 DDRB = 0x10;      // PORTB input
 PUCR_PUPBE = 1;    // PORTB pull enable
  //PTS = 0xFF;            // port S data default
 DDRS = 0x10;           // PortS DDR default
 REFDV = 0x40;     // XTAL=4MHz
 
 // Make sure we use the Xtal Oscillator
  //CLKSEL &= 0x7F;
 
  // Set Sys Clock to 32MHz by enabling PLL with a 4MHz Xtal
  //SYNR = 0x07;
  //REFDV = 0;
 
  // Enable the PLL
  //PLLCTL |= 0x40;
 
  // Wait until the PLL is stable
  //while(!(CRGFLG & 0x08));
 
  // Set PLL as Clock source, keep SYSCLK running in wait mode
  //CLKSEL = 0x80;
 
  /* SPI0BR: ??=0,SPPR2=0,SPPR1=0,SPPR0=0,??=0,SPR2=1,SPR1=1,SPR0=0 */
  //SPI0BR = 0x06;     // Baud = bus clock / 128
 
   /* SPI0CR1: SPIE=0,SPE=1,SPTIE=0,MSTR=0,CPOL=0,CPHA=1,SSOE=0,LSBFE=0 */
  SPI0CR1 = 0x44;   // Enable SPI as Slave, SS out auto
 
   /* SPI0CR2: ??=0,XFRW=0,??=0,MODFEN=0,BIDIROE=0,??=0,SPISWAI=0,SPC0=0 */
  SPI0CR2 = 0x00;   // prep Master Mode

  long outputCode;
  double voltage;
  unsigned char adcCode[5];
           
  PORTB = 0x10;
  while(!(PTS_PTS7))
   
      adcCode[0] = 0;
      adcCode[1] = 0;
      adcCode[2] = 0;
      adcCode[3] = 0;
      adcCode[4] = 0; 
      PORTB = 0x00;
     while(!(SPI0SR_SPIF));  // wait for SPI transmit ready
       adcCode[0] = SPI0DRL; 
     while(!(SPI0SR_SPIF));  // wait for SPI transmit ready
       adcCode[1] = SPI0DRL;     
     while(!(SPI0SR_SPIF));  // wait for SPI transmit ready                                                    
       adcCode[2] = SPI0DRL;
     while(!(SPI0SR_SPIF));  // wait for SPI transmit ready
       adcCode[3] = SPI0DRL;      
     while(!(SPI0SR_SPIF));  // wait for SPI transmit ready
       adcCode[4] = SPI0DRL;
              
     //outputCode = (((0xFF & 0x80) ? (0xFFL) : (0x00L)) << 16);
       
     outputCode = (long)(((((adcCode[2] & 0x80) ? (0xFFL) : (0x00L)) ) << 24)|((adcCode[2] & 0xFFL) << 16)|((adcCode[3] & 0xFFL) << 8)|((adcCode[4] & 0xFFL) << 0));
     
      voltage = outputCode * .0000004883;
 
  for(;;) {
      _FEED_COP(); /* feeds the dog */
     } /* loop forever */
     /* please make sure that you never leave main */     
   
  
}

0 Kudos
Reply
1 Reply

727 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi.

I don't understand how to reproduce your problem. Could you please send us more information:

1.    your CW version:
  - if you use classic version: Start the IDE and click on Help | About Freescale CodeWarrior. Click on Installed Products.Save all info displayed into a txt file and send it to me.
  - if you use eclipse version: Start the IDE and click on Help | About CodeWarrior Development Studio. Send me the version and build id.
2.    send the entire sample code folder(include mcp, prm,c...) in zip format to me.if your project is confidential, please create a new demo project and isolate the problem a demo code to me so that i can test it on my side directly.
3.      error screenshot.

I will go on checking your problem once I get feedback from you. Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply