Another 'Device is Secure' Issue (Solved)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Another 'Device is Secure' Issue (Solved)

2,055件の閲覧回数
Keith4DSmith
Contributor V

I am writing this post to add one more conversation to the 'Device is Secure' issue.

 

I had an issue with "Device is Secure" message when programming a Tower Board K60F120M

 

When I downloaded using the debugger, I got 'Device is Secure' ... message. RAM configuration was fine.

 

I have read several posts on this issue.

 

One said to apply a patch to version 10.3 of CodeWarrior.

I'm running version 10.5. The patch doesn't apply.

 

Another said to check a box in Component diaglogue for mass erase.

I don't have this dialogue for the K60F120M board I'm using.

 

Finally, one post attached a program to check that the Flash security bits haven't been set, bricking the board.

Next to use Flash Programmer/Mass Erase, and this is supposed to cure the problem. Not for me.

 

I am able to use the Flash Programmer pulldown in CodeWarrior to 'Mass Erase' and 'Flash File to Target'. No errors.

 

I am using a P&E Micro Multilink FX device, version 7.09 firmware.

 

The P&E dialogue (enabled in advanced settings of the debug configuration), reports Error 18 - Programming Error.

 

How did I 'cure' the 'Device is Secure' error?

 

I found I had selected the wrong K60 processor when I created a new project.

 

Build a project with the correct part, no "Device is Secure" issue.

ラベル(1)
0 件の賞賛
返信
1 返信

1,794件の閲覧回数
Keith4DSmith
Contributor V

Solved

0 件の賞賛
返信