Add MC9S12A64 Support to CodeWarrior for HCS12?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add MC9S12A64 Support to CodeWarrior for HCS12?

1,904 Views
zackeryarnold
Contributor I

Hi all,

I'm looking at the source for an old project designed to run on the MC9S12A64. I installed the necessary version of CodeWarrior but this specific micro isn't listed when I try to create a new project. Is there a way I can import this processor into CodeWarrior to continue with this process?

Thanks!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,826 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Zackery,

I wonder you use CW5.2 which doesn't support 9s12a64.

To work with 9s12a64, please download CW5.1 instead.

Attached video is for how to get CW5.1.

Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply