ARM7 Compile using Codewarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ARM7 Compile using Codewarrior

1,942件の閲覧回数
bsd9109
Contributor I

hello

My Company name is YURA CORPERATION.

I'd like to compile this project through the Codewarrior.

I'm using the ARM7 mcu in the making STMicroelectronics.

Could you explain why this error happen and i'd like to resolve this error.

thank you.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,888件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Sang,

Now CodeWarrior doesn't support 3rd party MCU. It only supports our own product.

Which version of CW do you work with?


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信