AN3034SW Error C2801 missing ';'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN3034SW Error C2801 missing ';'

2,914 Views
rachelsanford
Contributor I

I'm trying to run the sample code from document AN3034 "Using MSCAN on the HCS12 Family". The code is in document AN3034SW. Both of these documents are provided by NXP.

I did modify an include statement and the pragma Link_Info so that it matched the development board I am working with, the MC9S12DG256 development board.

 

I tried to compile the code and I am getting "Error C2801 ';' missing", but it seems like I have all of the appropriate semicolons. It is also strange because the error happens on 4 very similar lines of code. It is during the CANInit function that this occurs. The CANInit function is shown below. The full code is attached. The code that I copied and minimally modified is from AN3034SW. The lines causing errors are in RED. They all cause the same error: "Error C2801 ';' missing". I am using CodeWarrior 5.9.0.

//CANInit Function

void CANInit(void){

  CAN0CTL0 = 0x01;  //Enter initialization mode

                     

  while(!(CAN0CTL1&0x01)){}; //Wait for initialization mode ACK

  CAN0CTL1 = 0xA0;  //Enable MSCAN module and Loopback Mode

  CAN0BTR0 = 0xC7;  //Synch Jump = 3Tq clock cycles (re calculate?)

  CAN0BTR1 = 0x3A;  //Set number of samples per bit, TSEG1 and TSEG2

  CAN0IDAC = 0x10;  //set four 16-bit filters

 

  //Acceptance Filters

  CAN0IDAR0 = ACC_CODE_ID100_HIGH; //16-bit filter 0

  CAN0IDMR0 = MASK_CODE_ST_ID_HIGH; //Accepts Standard Data Frame Msg  ERROR Missing ;?

  CAN0IDAR1 = ACC_CODE_ID100_LOW; //with ID 0x100

  CAN0IDMR1 = MASK_CODE_ST_ID_LOW;

 

  CAN0IDAC = 0x10; //Not sure why this is twice in code

 

  CAN0IDAR2 = 0x00; //16-bit filter 1

  CAN0IDMR2 = MASK_CODE_ST_ID_HIGH; //Accepts standard Data frame msg

  CAN0IDAR3 = 0x00;   //with ID 0x000

  CAN0IDMR3 = MASK_CODE_ST_ID_LOW;

 

  CAN0IDAR4 = 0x00; //16-bit filter 2

  CAN0IDMR4 = MASK_CODE_ST_ID_HIGH; //Accepts standard Data frame msg

  CAN0IDAR5 = 0x00;   //with ID 0x000

  CAN0IDMR5 = MASK_CODE_ST_ID_LOW;

 

  CAN0IDAR6 = 0x00; //16-bit filter 3

  CAN0IDMR6 = MASK_CODE_ST_ID_HIGH; //Accepts standard Data frame msg

  CAN0IDAR7 = 0x00;   //with ID 0x000

  CAN0IDMR7 = MASK_CODE_ST_ID_LOW;

 

  CAN0CTL0 = 0x00; //Exit initialization mode request

 

  while((CAN0CTL1&0x01)!=0){}; //Wait for normal mode

 

}  //end void CANInit

Original Attachment has been moved to: main.c.zip

Labels (1)
0 Kudos
Reply
1 Reply

2,320 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Rachel,

I have checked your file  , there is some spelling error for macro definition .

pastedImage_0.png

pastedImage_1.png

I changed them  , please check the attachment .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply