9S12x Interrupt vector address in .prm file or in code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9S12x Interrupt vector address in .prm file or in code?

ソリューションへジャンプ
3,398件の閲覧回数
jcdammeyer
Contributor III

I've done several projects on the 9S12XDP512 and in each case I've used the .prm file to specify the names of the interrupt handling functions.

 

/* use these definitions in plane of the vector table ('vectors') above */

VECTOR 0 _Startup /* reset vector: this is the default entry point for a C/C++ application. */

//VECTOR 0 Entry  /* reset vector: this is the default entry point for an Assembly application. */

//INIT Entry      /* for assembly applications: that this is as well the initialization entry point */

VECTOR ADDRESS 0xFF78     PIT1_ISR            

VECTOR ADDRESS 0xFF7A     PIT0_ISR            

VECTOR ADDRESS 0xFFD6     COM1Interrupt

VECTOR ADDRESS 0xFFD4     COM2Interrupt

 

This is all based on the original example code from the Softec Development board I started with.

The linker fills in the rest of the table with FFFF so a spurious interrupt should reset the application since the entry at that RESET vector is 0xC000.

Is there a better way to do this or should I care?

 

In the timer.c file I have:

#pragma CODE_SEG __NEAR_SEG NON_BANKED

interrupt void PIT0_ISR(void) {

     TickCount++;

PITTF = 0x01;
}     

#pragma CODE_SEG DEFAULT

 

In order to access the variable TickCount I disable interrupts since TickCount is a 16 bit variable and could change between reading it and clearing it.

// disable timer interrupts

    PITINTE &= DELAY_TIMER_DISABLE;

    // Update local copy.

    t_Delay = TickCount;

    TickCount = 0;

    // re-enable timer interrupts

    PITINTE |= DELAY_TIMER_ENABLE;

 

Any comments on the above.  Is there anything unique in the 9S12 family that I'm missing here?  Specifically when I see the comments in the .prm file about OSEK etc.

ENTRIES /* keep the following unreferenced variables */

    /* OSEK: always allocate the vector table and all dependent objects */

    //_vectab OsBuildNumber _OsOrtiStackStart _OsOrtiStart

END

 

Thanks

John

 

 

 

 

.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,848件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi John. !

the interrupt vector address is correct in your code.

please perform interrupt per attached technical note.

==================================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,849件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi John. !

the interrupt vector address is correct in your code.

please perform interrupt per attached technical note.

==================================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 件の賞賛
返信