9S08AW60 as USB host using MAX3421E as host controller interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

9S08AW60 as USB host using MAX3421E as host controller interface

1,594 次查看
frédéricleblanc
Contributor I

Hello ,

 

I apologize for my poor english langage.

I try to use a 9S08AW60 as a simple host for controlling printer. The interface is a Maxim MAX3421E Host controller. Communication is done trough SPI. Power supply is 5V for microcontroller and 3.3V for Max3421 and i've inserted an ADG3304 for voltage "transformer". I have many difficult in using SPI to send setup  to the MAX3421. I can  see activity on USB like  busreset, SOF each ms, after i have sent order to sent it, adress change "Set Adress". Despite this i can't read anithig in return (interrupt registers, receive fifo...)

 

Help, i search an idea to control and fix my bugssssss.

 

Thank You and Best regards

 

Fred

标签 (1)
0 项奖励
回复
0 回复数