68HC908AS/AZ + USB-ML-MON08 + CW for MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

68HC908AS/AZ + USB-ML-MON08 + CW for MCU

2,216 Views
rw_ae2i
Contributor I

Hello everybody,


We are trying to prepare a development environment for a 68HC908AS/AZ CPU.


New to Freescale, we are wondering what kind of hardware and software we need.


We have selected USB-ML-MON08 as programmer/debugger, and we are wondering if CodeWarrior for MCU would be compatible to compile, load and debug software ?


We have looked at v6.3 and v10.6 and we have questions on both :

   - is v6.3 compatible with Multilink MON08 Rev C ?

   - can v10.6 help program HC08 CPUs (we haven't found them in any list) ?


Thanks in advance

Labels (1)
0 Kudos
Reply
3 Replies

2,070 Views
rw_ae2i
Contributor I

Thank you all for your answers

We understand your concern about HC08 not being produced anymore, but this is to change and improve an old application, that is why we go back to old software

0 Kudos
Reply

2,070 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Regis.

Yes, to work with 68HC908AS/AZ, we need to use USB-ML-MON08 and CW6.3.

CW6.3 is compatible with Multilink MON08 Rev C.

CW10.6 can’t support HC08 device. For 8bit, it support HCS08 only.

=======================================

this answer is for you. if it helps, please click on "Correct Answer" button. thanks!

Best Regards,

Zhang Jun

0 Kudos
Reply

2,070 Views
Rick_Li
NXP Employee
NXP Employee

Hello Regis Wernet,

regarding your questioin:

- is v6.3 compatible with Multilink MON08 Rev C ?

YES, CW v6.3 compatible with Multilink MON08 Rev C, but CW v6.3 only works in Windows XP, it does not work in Win 7 or later system.

CW v6.3 can also be used to program HC08 MCU.

   - can v10.6 help program HC08 CPUs (we haven't found them in any list) ?

NO, CW v10.6 does not support HC08 MCU.


PS: FSL HC08 family is not produced any longer, if you want to develop a new application, then, I would suggest using 32 bits Kinetis serial MCU.

0 Kudos
Reply