64 bit install

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

64 bit install

1,718 次查看
dangela
Contributor I

How do I install CW on my PC running Windows 8.1? I get a popup window that says,

"CodeWarrior Development Studio For ColdFirev7.2 does not support 64 bit OS."

 

I tried changing compatibility mode to Windows 7 and got the same window.

标签 (1)
0 项奖励
回复
1 回复

1,391 次查看
TICS_Fiona
NXP Employee
NXP Employee

The Classic CodeWarrior does not support Windows 7 or Windows 8, the latest version 7.2 only supports Windows XP and Vista(32-bit).

The first version for Coldfire which officially supports Windows 7 is Eclipse version v10.0, and now the latest Eclipse CodeWarrior version is 10.6: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

There is a workaround to install CW for Coldfire v7.2 on Windows 7 64 bit in XP mode. This mode is available only on Win 7 Professional. It’s a XP emulation.

However there is a P&E driver issue. Customer must download the V10 from P&E web site too.

For details, please refer to:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN3936.pdf

However, this is un-official recommended installation. By default we recommend use to switch to Eclipse CodeWarrior.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复