56800

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

56800

1,858 Views
hrachsalmasian
Contributor I

Hi

  I have recently bought 56F83EVM kit   PN:CWX-568-SE  I have installed  it.

Does it need to licensing & activation ?

  I can not access to (processor expert example stationery)  so I can not find sample programs . what should i do ?

thank you

BR

Hrach

0 Kudos
Reply
2 Replies

1,671 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Besides Stan,  processor expert example stationery demo code can be found under

C:\Freescale\CodeWarrior for DSC56800E v8.3\Stationery

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,671 Views
stanish
NXP Employee
NXP Employee

Hi,

You installed Free Special Edition version of CodeWarrior that limits some features + code size. It does not require any activation or license. It has limited features.

  

You can try to download and install the evaluation version - 30 days without any limitations (Professional edition):

http://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-568-EX 

Stan

0 Kudos
Reply