0 object files loaded in console window when debugging in Codewarrior v10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

0 object files loaded in console window when debugging in Codewarrior v10.6

1,820 Views
arthivenkatasub
Contributor III

Hi,

I just took an example code of LSM, MPC5643L and I used codewarrior v10.6 as IDE. Then, I build it; clicked on debug button and select the corresponding file to flash. I didn't find any .abs file, so i selected .elf file.

The program got erased and also started flash. But, at the end it displayed as zero files loaded.

Can anybody guide me?

This is the first time, I am using codewarior v10.6. I used user manual for reference.

Regards,

Arthi Venkatasubramanian

2 Replies

1,604 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please share the project? I need to check this on my side.

Which debug probe you use?

Regards,

Martin

1,604 Views
arthivenkatasub
Contributor III

Hi,

Thanks for your reply. I just changed debug configuration settings and it is working. I am able to run the program.

Regards,

Arthi Venkatasubramanian

0 Kudos
Reply