windows 10 iot boot issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

windows 10 iot boot issue

2,899件の閲覧回数
puneeth989
Contributor I

hi,

      I am trying to boot windows 10 iot on imx6q. But it is freezing in #KDTARGET: Refreshing KD connection. Please give any solution for this. I have attached the boot log.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,731件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

May I ask, do you happen to get anything on your display?

You should see Windows logo after U-boot hands off to UEFI.

 

Message KDTARGET: Refreshing KD connection

This message is the Windows kernel debugger is attempting to connect over serial, which indicates you are making it into Windows. 

 

Thank you,

Best regards,

Aldo.

0 件の賞賛
返信

2,731件の閲覧回数
MengJu_Lin
NXP Employee
NXP Employee

nxf46838

I have a similar issue.

I use i.MX8M Mini EVK with W1860_1_0_1_NXPEVK_iMX8M_Mini_2GB_TestOEMInput-xml-Release.ffu flashed to SD card.

The attach files are screen shots of tera term and HDMI display.

It complains no IP address and stoppped. I don't have ethernet connection. How can I setup WIFI connection?tera term.PNGwindows.jpg

0 件の賞賛
返信