unable to debug....

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unable to debug....

2,144件の閲覧回数
koka
Contributor I

hi...

i'm new to DSP56800 chip...

i'm checking the examples in the softwares...

in that if i'm creating the project by DSP56800X EABI stationery....

i'm viewing the code, compiling and linking.....but i'm unable to debug...

i'm getting the error like " CCSprotocolplugin : unknown protocol error"

is there any need of connecting Hardware for checking the output.........and is there any need of installing any plugins for getting the output...

so what i have to do...

 

please help me as fast as possible.....

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,244件の閲覧回数
J2MEJediMaster
Specialist I

The Quick Start Guides that accompany the software usually give you information on connecting the target board to the computer. Also, you need to go to the project's settings panels (type Alt+F7) in the IDE to display the settings panels. Check the debugger settings panels (there are several) to see that the debugger communications is configured proerly.

 

---Tom

0 件の賞賛
返信