__start.c .the program stucks in this file..

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

__start.c .the program stucks in this file..

1,050件の閲覧回数
hrishikesh23
Contributor I

Dear All,

 

               Please need your help in resolving this isssue. I am Using Code warrior IDE version 5.9.0. On both Windos Xp as well as Win7. I have MPCHPCN: Argo Novis Motherboard of freescale MPC8641D...I am trying to laod the code into the Core. The code gets downloaded succesfully but gives Error..saying

Program "debug.elf (chain position 1, core #1)" is executing.
Choose Break from the Debug menu to stop it.

 

Please let me know if anyone has experienced this issue and sorted out...i have treid using two different debuggers but has resulted in same result.

 

 

 

Thanks and regard

Hrishikesh.

ラベル(1)
0 件の賞賛
返信
1 返信

878件の閲覧回数
hrishikesh23
Contributor I

No One has faced this Problem.... ???????????

0 件の賞賛
返信