signal when debugger crashes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

signal when debugger crashes

2,115 Views
mel
Contributor I

The debugger seems to crash randomly.

If it crashes while I have a motor in boost it burns out the board.

Is there a signal from the processor that will let me know when the debugger

crashes? I am using codewarrior 7.3 on the 56f8357.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

701 Views
Oppie
Contributor I
Let me expand on this.
There are some high power processes under control of the processor. When emulation stops, we need a graceful way to shut down the power processes so that the board does not burn up.
 
Is there some hardware method to flag when emulation stops on a breakpoint or emulation failure?
 
codewarrior 7.3 on the 56f8357.   Emulating through the parallel port using OCDemon 'wiggler' jtag converter.
 
TIA
0 Kudos
Reply