regarding demo board ...........

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

regarding demo board ...........

1,847件の閲覧回数
ellendula
Contributor I
hi...
i installed CW_DSC56800E_V8_2_3_SE ....
and i downloaded 56F800 demo board (Embedded SDK-Targetting MOtorola 56F800 Demonstration Board) manual and i downloaded 56F800 Demonstration Board User Manual......
so in that i'm seeing .....
" ...\nos\applications\quadtimer\quadtimer.mcp" what is that ... in the double quotes represents ...i unable to find that .mcp file...
so please tell me ...how can i see demo board applications......in the code warrior....
please help me....
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

946件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

 

SDK is very old.

There are some examples under the installation.

Please have a look to:

 \CodeWarrior for DSC56800E v8.2.3\(CodeWarrior_Examples)

 \CodeWarrior for DSC56800E v8.2.3\Stationery\Processor_Expert

 \CodeWarrior for DSC56800E v8.2.3\Stationery\Processor_Expert_Examples

 

I recommend you to have a look to:

 \CodeWarrior for DSC56800E v8.2.3\Stationery\Processor_Expert_Examples\DemoApplications

 

Hope this will help you.

Regards

Pascal

0 件の賞賛
返信