"Internal error: DoSuspend" message

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"Internal error: DoSuspend" message

3,122件の閲覧回数
CONDER
Contributor I
Hi, dear all,

I have a question on CW debugging.
While debugging under CW, sometimes my program gets "frozen", i.e., it stops execution but not return. Pressing "break" botton gives me following message:
Internal error: DoSuspend
Thread error

Could someone give me a hint what may cause this problem? Thanks in advance.

Regards,

CONDER
ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,450件の閲覧回数
CrasyCat
Specialist III
Hello
  Which CPU are you targeting (HC08, HC12, Coldfire, ...)?
  Which version of CodeWarrior are you using ?
    To retrieve that info:
      - Start IDE
      - Select Help -> "About Freescale CodeWarrior"
      - Press on "Installed Products"
      - You will see CodeWarrior version info into the title bar.
  Which cable are you using to connect to your target board( Multilink, USBTAP, ...)?
 
CrasyCat
0 件の賞賛
返信

1,450件の閲覧回数
CONDER
Contributor I
Hi, CrasyCat,

Thanks for you reply.

I'm using MSC8122 DSP and using USBTAP to connect to the board.
The CodeWarrior version is:
CodeWarrior StarCore Compiler (Windows), Engineering Build 18
CodeWarrior Development Studio for Freescale StarCore DSP Architectures, Version 2.7.2, Update Build 2
IDE Version: 5.7.0 Build 1996


Regards,

CONDER
0 件の賞賛
返信

1,450件の閲覧回数
CrasyCat
Specialist III
Hello
 
Only case I get this message was when I was using a wrong register configuration file in my project.
Make sure the configuration file you use in the SC100 Debugger Target panel is correct.
 
If this does not help, I would recommend you to submit a service request through our web page to get support people get a look at it.
Specify board, CodeWarrior version and connection you are using when submitting the SR..
 
CrasyCat
0 件の賞賛
返信