progamming power pc mpc5200b

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

progamming power pc mpc5200b

Jump to solution
1,768 Views
j_tag
Contributor I

hello,

 

 

i want to start learning progamming. i have some  board with the power pc mpc5200b  with external flash memory.

 

 

i have one code warrior usb tap. but i dont have the software and usb drivers to progamming the mpc5200b core.

 

 

 

wich  software do i need?

 

 

 

best regards

Labels (1)
0 Kudos
Reply
1 Solution
1,526 Views
J2MEJediMaster
Specialist I

You will want to download CodeWarror for mobileGT, which supports the processor type. Information about these tools and a download link can be found on this web page.

 

---Tom

 

 

 

View solution in original post

0 Kudos
Reply
2 Replies
1,527 Views
J2MEJediMaster
Specialist I

You will want to download CodeWarror for mobileGT, which supports the processor type. Information about these tools and a download link can be found on this web page.

 

---Tom

 

 

 

0 Kudos
Reply
1,526 Views
j_tag
Contributor I

hello,

 

 

 

thanx tom for the download link!  after i downlaod the the software i cant connect to my core.

 

 

 

target core:mpc5200b habanero connect to code warrior usb tap.

 

 

i download the datsheet from the mpc5200b. and use the follow pins: use 16 pin j-tag cop connector)

 

BO4 j-tag tck

 

A02 j-tag tdo

 

AO3 j-tag tdi

 

A04 j-tag tms

 

A14 sreset

 

B13 hreset

 

 

my target dont support B03 j-tag trst. and i dont have CKSO,QACK on the board

 

 

when i go to:hardware diagnostic  and i try to connect to the core( test begin scoop loop) i dont see the run/pause led working. all the time the rx/tx led is working and stay green.

 

 

i hope i provide all the information to get some help.

 

 

 

bet regards.

 

 

 

 

0 Kudos
Reply