problems with freemaster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problems with freemaster

2,653 Views
lijiacui
Contributor I

hello!

I want to use SPI to receive datas from the sensor and hope to  show data on PC by PC_Master. Does the project work?

 

I debug the example for PC_Master 56F8357,it works.But the same program on 56F8346 does not work and does not generate the pmp files,why?

 

Thank you very much!

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,493 Views
lijiacui
Contributor I

The program used on 56F8346 can make and debug ,but can not generate the pmp files .why? thank your answer ,Tom!

0 Kudos
Reply

1,493 Views
lijiacui
Contributor I
Is there anyone who can help me?
Thank you!
0 Kudos
Reply

1,493 Views
J2MEJediMaster
Specialist I

There's not much detail to "it does not work" to go on here. Are you using the exact same code for the 56F8346 that you used on the 56F8357? There are probably enough differences between the two processors (certain I/O pins, or a different clock frequency) so that the code does not work.

 

---Tom

0 Kudos
Reply