need a start

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

need a start

1,490 次查看
olderone
Contributor I
hello verybody
i got a problem. i used dsp56k long time  ago and i used it without problem.
 
few days back i got mc56f8367evme board.  i am confused where to start. any body can give me some direction  that can be book or df or anything..it would be great if there is a step step instruction and examples.
thanks
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

517 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

 

I recommend you to download the last version :

CodeWarrior Development Studio for Freescale 56800/E Digital Signal Controllers Version 8.2.3

You can download this version on our web site via the link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

For details please have a look in:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC&tab=In-Depth_Tab

In the download tab you can download the Special Edition or the Evaluation.

The Special edition contains the special edition license limited to 32 kb of Code.

We recommend you to download the Evaluation edition.

A Professional Evaluation license is provided for first 30 days.

After 30 days the product will function at the Special Edition level.

If you need another version of the license please contact your local distributor.

You can purchase it directly from the web site too.

 

We changed the pricing and packaging structure for Codewarrior Tool.

Now there are 4 suites:

special (free version)

basic

standard

professional

Please refer to the link for details:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127262E703BC5

Go to the www.freescale.com and click on My Freescale.

After you were logged, select CodeWarrior Licensing under MY Secure Application.

In the new dialog you can manage your license file.

 

Keep in mind you can have several versions installed on the same PC.

There is only one restriction: install them on separate folder.

If you're using an old version, please backup your project before to try it with this new version.

If you will meet some compatibility issue you could back to the older version without problem.

 

For the patches, please use the link :

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882

 

 

There are some examples delivered with the tool installation.

Please refer under the folders:

 - \(CodeWarrior_Examples)

 - \Stationery

 

A quick start manual is available under:

 \Help\PDF\56800x_Digital_Signal_Controllers_QS.pdf

 

Hope this will help you.

Pascal

0 项奖励
回复