interrupt vector table for MC9S08RE16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

interrupt vector table for MC9S08RE16

2,214 Views
stevec
Contributor III
Can someone tell me how to put an interrupt vector table into CodeWarrior. I'm using an MC9s08RE16. I already have some code written but now require an interrupt driven timer. I've tried using the Device Initialiser but the linker generates error L1119: Vector allocated at absolute address 0xFFFE overlaps with sections placed in segment .absSeg64. Is this because the _Startup vector is being set in the Start08.c code and the MCUinit code? I started the code without using Device Initialiser but called it up to put in the timer interrupt. Is this allowed?

Steve


Message Edited by J2MEJediMaster on 2007-06-22 09:42 AM
Labels (1)
0 Kudos
Reply
1 Reply

742 Views
CompilerGuru
NXP Employee
NXP Employee
Probably the problem is that the reset vector is defined both by device initialization and explicitely in the prm file.
If you use device initialization, comment the VECTOR 0 entry in the prm file.

Daniel
0 Kudos
Reply