display the FFT in a diagram under CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

display the FFT in a diagram under CodeWarrior

2,742 Views
cimbom
Contributor I

Hello,

 

I know that the CodeWarrior can display the FFT in the diagram but I unfortunately do not know how and where. Where can I have displayed the FFT under CodeWarrior in a diagram?

 

Thanks

Labels (1)
0 Kudos
Reply
3 Replies

890 Views
J2MEJediMaster
Specialist I
I assume you're using a DSP of some sort, and perhaps CW 6.4, but I'm guessing.

Just a friendly reminder: please enter the MCU type and CodeWarrior version in your post's subject line so that forum visitors with the appropriate experience will notice your question and try to answer.

---Tom


0 Kudos
Reply

890 Views
charanreddy
Contributor III

Hi

I am trying to implement FFT transform in FRDM KL25Z which is cortex M0+ using codewarrior. I have downloaded the CMSIS library and tried the procedures mentioned in the community. But i am not able to implement them successfully, i am getting some errors even when i tried to implement some inbuilt example codes. Can any one help me with this issue.

Regards,

Charan Kumar.

0 Kudos
Reply

890 Views
trytohelp
NXP Employee
NXP Employee

Hi Charan,

This post is very old based on CW for DSC tool.

You're using Kinetis with probably CW for MCU V10.6.

Can I recommend you to create a new post for this question ?

Please provide more details regarding the dev tool and other stack/library you're using.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply