code not saved

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

code not saved

跳至解决方案
2,793 次查看
Greeny
Contributor I

Hi all,

 

i have a problem with COdewarrior and the beans.

I implemented 2 Timer Output Beans via Processor Expert. Now when i change the corresponding TOx.c file it´s all right and working fine. BUT when i close Codewarrior and load the project again the changes done to the .c file are gone. Seems that PE is updating the .c files when project is loaded ?!

 

Can i change this option somehow ?

 

greetings

标签 (1)
0 项奖励
回复
1 解答
1,774 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

the behavior that is described in your issue is correct. Generally it is not recommended to modify the code generated by Processor Expert manually. However to avoid your problem you can switch on the "Don´t generate the bean module" menu command in bean´s pop-up menu.

 

Please see the Processor Expert help chapter Application design / Code generation and usage / User changes in generated code.

 

best regards
Vojtech Filip
Processor Expert Support Team

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,774 次查看
Greeny
Contributor I
Thanks a lot !
0 项奖励
回复
1,775 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

the behavior that is described in your issue is correct. Generally it is not recommended to modify the code generated by Processor Expert manually. However to avoid your problem you can switch on the "Don´t generate the bean module" menu command in bean´s pop-up menu.

 

Please see the Processor Expert help chapter Application design / Code generation and usage / User changes in generated code.

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复