can I run codewarrior in my PowerBook G4 with linux OS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can I run codewarrior in my PowerBook G4 with linux OS?

1,833件の閲覧回数
WuXuDong
Contributor I
I find there are 3 rmp in codewarrior(CWS-PPC-LLPLT-CX) install folder:
1. mtwk-lnx-powerpc-linux-gnuspe-gcc-3.4.3-e500-glibc-2.3.3-spe-0.28-4.i686.rpm
2. mtwk-powerpc-gcc-2.95.3-glibc-2.2.1-0.28-2.i686.rpm
3. mtwk-powerpc-gcc-3.3.2-glibc-2.3.2-0.28-1.i686.rpm

it seems that they are all designed for x86 machine, can I install them and run codewarrior in my PwerBook G4?

BTW, where can I download following package :
mtwk-lnx-powerpc-gcc-3.4.3-glibc-2.3.3-0.28-1.ppc.rpm

who can help me ? Thanks .
ラベル(1)
0 件の賞賛
返信
1 返信

578件の閲覧回数
J2MEJediMaster
Specialist I
No, you can't. The three files you mention consist of x86 code and thus only execute on a x86-based system. As the Powerbook G4 is PowerPC-based, these files won't execute on that particular laptop.

---Tom
0 件の賞賛
返信