auto version in CW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

auto version in CW

1,594 Views
Nouchi
Senior Contributor II

Hello,

 

I'm not familiar with Eclipse and CW10 indeed (not yet), is there any auto versioning plugins for eclipse (or CW10)?

 

 

Emmanuel

Labels (1)
0 Kudos
Reply
2 Replies

1,093 Views
CrasyCat
Specialist III

Hello

 

I am not sure what you are looking for?

Are you looking for plug ins to integrate Version Control software in CodeWarrior V10.x?

 

You can find plug-ins to extend CodeWarrior framework on
  www.eclipseplugincentral.com
Just make sure the plug ins are compatible with the Eclipse version number.

To check Eclipse version number:

    - Select Help > About CodeWarrior development Studio

    - In the About CodeWarrior Development Studio dialog click on the icon which has tool tip starting with  Eclipse.org.

    - Check the version number for the feature Eclipse Platform there. If it starts with 3.4 you can take any plug ins

       compatible with Eclipse V3.4.

 

CrasyCat

0 Kudos
Reply

1,093 Views
Nouchi
Senior Contributor II

Hello,

 

I just want something increasing a build number string, but your link is very useful.

 

Thanks CrasyCat

0 Kudos
Reply