Windows 7 Unhandled Exception

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows 7 Unhandled Exception

ソリューションへジャンプ
33,936件の閲覧回数
nonarKitten
Contributor II

When starting the IDE in Windows 7, the proram will work fine until a project is loaded at which point it will report an error:

 

CodeWarrior encountered an unhandled exception 0xc0000005 at address {different each time} (The memory at address {different random address} could not be read)

 

Location: IDE.EXE:{same as the first random address}

 

Crash dump written to MEM_FREE.b2830.20090320.122156A.dump

 

Choose 'Abort' to end the program, 'Retry' to debug, or 'Ignore' to continue (at your own risk!)

 

Abort will kill it, Retry will cause it to be unresponsive, and Ignore just brings the same error back up a few times until I get this:

 

Generic Error 32770. An unknown error has occured.

 

Neither running as Administrator nor taking ownership of the Program Files folder seems to help.

ラベル(1)
1 解決策
14,933件の閲覧回数
Audi
Contributor II

I found this work-around. . .

 

Again, I am using 32-bit Win7 Pro.  I run CW with the "Disble desktop composition" enabled (checked).  You can find that option on the Compatability tab of CW's Properties dialog.

 

 

元の投稿で解決策を見る

25 返答(返信)
1,695件の閲覧回数
Teto
Contributor I

Thanks Audi, it work fine

0 件の賞賛
返信
1,695件の閲覧回数
jajomafa
Contributor I
Hello, I am having the exact same problem with CW v6.3 and Windows 7 x86. Have you found any solution?
0 件の賞賛
返信
1,695件の閲覧回数
CrasyCat
Specialist III

Hello

 

- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.

 

CrasyCat

0 件の賞賛
返信
1,695件の閲覧回数
nonarKitten
Contributor II

Codewarrior 6.2.1 (fully patched) for Microcontrollers (RS08 specifically). 

 

I have a good machine, and I'd hate to waste a lot of RAM having to run Vista 32-bit. So far I've tried Vista 64-bit and Windows 7, neither of which will alllow CodeWarrior to run. Might look at trying to run a 32-bit Windows on 64-bit Windows just for CodeWarrior - sad that I have to do that. The only common changes for both have to do with the absence of the 16-bit layer, no support for 32-bit drivers, strict kernel protection and enforced driver signing. Not sure which/where would be causing the problem.

0 件の賞賛
返信
1,695件の閲覧回数
CrasyCat
Specialist III

Hello

 

This looks to be related to either your project r our installation.

I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.

Also attach the crash dump file (MEM_FREE.b2830.20090320.122156A.dump)

 

CrasyCat

0 件の賞賛
返信