Where is the stack size setting in eclipse ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the stack size setting in eclipse ?

1,369 Views
SecondTechCo
Contributor IV

 i have found it in project.lcf but not in the eclipse IDE.   I have read one other post which says it is in the build settings CPU but I dont see it there.

Labels (1)
2 Replies

1,127 Views
CrasyCat
Specialist III

Hello

 

   I assume you are talking about the size of the stack used to run the application. Am I right?

 

  This is done differently according to the processor you are targeting.

  - Which CPU are you targeting (HC08, HC12, Coldfire, ..)
  - Are you using CodeWarrior v10.x (Eclipse based) or an earlier release of CodeWarrior?

 

CrasyCat

1,127 Views
SecondTechCo
Contributor IV

I figured out where it was. Eclipse 10.2.  Thanks

0 Kudos
Reply